×

PC Control These demos and projects allow the robot to be controlled via a computer.

ArbotiX Commander Control - These demos and projects control the Robot using the ArbotiX Commander, the handheld Arduino based remote control.

Direct Control - These demos and projects control the Robot directly from sensors connected directly to the Robot's control board.

Pose Control - These demos and projects allow you to create and playback a sequence of poses.

Serial Control - These demos and projects control the robot using a serial packet protocol.

Standalone - These demos and projects are deisgned to let your robot function without a computer or additional microcontroller.

Wireless Control - These demos and projects allow you to control the robot wirelessly - usually by replacing the Serial Connection with XBee modules.

Reference - These articles have technical details regarding the control and operation of the robot.

×

More info here

PhantomX Robot Turret Projects

  • Analog Joystick Control for the PhantomX Robot Turret

    Description

    mt_ignore
    Standalone
    mt_ignore
    Direct Control

    The easiest way to control the Robot Turret is via the included joystick. This page will show you how to wire your joystick to your ArbotiX robocontroller and what code to load onto the ArbotiX Robocontroller.

    This code for this demo project will read the analog value from the joysticks, convert the raw value into a value ready for the DYNAMIXEL servos, and then write the positions to the servos. The code will also impose angle limits on the pan/tilt system and offer variable speed, adjustable by the user.

    The vertical joystick will control the tilt servo while the horizontal joystick will control the pan servo. These motions can be swapped in code, or by physically swapping out the 2 sensors. This code can work with a wide variety of joysticks. It can also work with other analog sensors, though some code modifications may be necessary depending on the desired behavior.

    Read More
  • DYNAPose - DYNAMIXEL/ArbotiX Pose Tool

    Description:

    mt_ignore
    Pose Playback
    mt_ignore
    PC Control

    All the InterbotiX robots turrets, arms, and crawlers use DYNAMIXEL servos. These servos all have positional feedback, allowing the ArbotiX-M Robocontroller to read the current position of each servo. This makes it possible to physically pose an InterbotiX robot, then capture the positions for each servo, allowing the user to save/capture the current pose. By capturing multiple poses, a user can create a sequence that can be repeated.

    This firmware does not use any Inverse Kinematic calculations to position the servos - it simply moves the servos to a pre-set position. Please see the 'Demo' section for your Robot for more information on code examples that us IK engines.

    Read More
  • LIDAR Lite Mapping with DYNAMIXEL Servos

    This demo will show off the capabilities of the LIDAR Lite by rotating the LIDAR lite and using the data to create a visual map of the room. This demo will require Google Chrome to be installed on your computer.

    Read More
  • Nifty Robot Neck & Vision System

    Created by Mewgen --- Project Page

    Description:

    User Mewgen has connected his PhantomX Robot Turret to an Asus Xtion to make a 2 Degree of Freedom 3D Camera.

    Mewgen has written a custom C++ / QT application that allows a user to control the robot and monitor its camera. This PC application sends data over a serial port to the ArbotiX Robocontroller on the Turret. The ArbotiX then sets the servo's position based on the command from the PC. The ArbotiX is able to do this running the stock ROS Arduino firmware, turning int into a pass-through device.

    This is a great example of how a simple 2-servo robot can be very useful, giving a 3d camera the freedom to scan whole rooms or objects. This kind of robot could also be adapated to a cralwer/rover, increaing the range that the robot can see while standing still.

    This is also a great example of using InterbotiX robots attached to an external device. Any InterbotiX robot can be controlled on the servo-level, using the ArbotiX Robocontroller as a pass through device. Alternativeley, all of the InterbotiX Robots will respond to ArbotiX Commander style packets, giving the user access to various functions and IK engines that we have built for the InterbotiX robots.

    Read More
  • Robot Turret Matlab Controller

    Created by Mewgen --- Project Page

    Description:

    User Mewgen created a Matlab controller for the PhantomX Robot Turret.

    Mewgen has written a custom firmware for the ArbotiX to allow for communication with his custom PC controller. The PC controller is written in matlab.

    This is another great example of how easy the ArbotiX robocontroller makes it to control DYNAMIXEL servos from a computer. Whether you want to make a custom firmware for the ArbotiX, or use one of our stock Arduino based firmware examples, the InterbotiX line of robots makes working with external devices and applications a breeze.

    Read More
  • Untethered Pose Playback with DYNAMIXEL/ArbotiX

    Description:

    mt_ignore
    Pose Playback
    mt_ignore
    PC Control
    (Setup Only)
    mt_ignore
    Standalone

    The ArbotiX-M Robocontroller can be used to easily 'play' a sequence of poses on DYNAMIXEL servos. These poses can run automatically, triggered by an outside input (like a pushbutton) or integrated into more advanced code.

    This tutorial can be used in conjunction with the DYNApose tutorial. The DYNApose tutorial will help you to capture a series of poses while this tutorial will help you integrate those poses into new code.

    This firmware does not use any Inverse Kinematic calculations to position the servos - it simply moves the servos to a pre-set position. Please see the 'Demo' section for your robot for more information on code examples that use IK engines.

    Read More
  • Virtual Commander - Generic Software Robot Control

    Description

    mt_ignore Wireless
    (Optional)
    mt_ignore
    Serial Control
    mt_ignore
    PC Control

    The Virtual Commander software is a piece of software designed to mimic the ArbotiX Commander. This is a small demo application written in Processing/Java. This application allows you to control InterbotiX robots as if it were connected to a real ArbotiX Commander as if it were connected to a real ArbotiX Commander. This can be very handy for rapid development, as you can program and control the ArbotiX over the same USB-FTDI connection, switching back and forth between the Arduino IDE and the Virtual Commander

    Read More
  • Wireless Handheld Control for the PhantomX Robot Turret

    Description

    mt_ignore
    Wireless
    mt_ignore
    Serial Control
    mt_ignore
    ArbotiX Commander Control

    The PhantomX RobotTurret can be controlled wirelessly via the ArbotiX Commander. In this demo, the ArbotiX Commander's joysticks will be mapped to the pan/tilt servos, and the pushbuttons will move the turret to pre-set positions.

    Users can modify the ArbotiX Robocontroller firmware in a variety of ways. The speed of the servos can be changed and the preset positions can be altered. Users can even trigger digital outputs (like relays) based on ArbotiX Commander input.

    Read More