×

PC Control These demos and projects allow the robot to be controlled via a computer.

ArbotiX Commander Control - These demos and projects control the Robot using the ArbotiX Commander, the handheld Arduino based remote control.

Direct Control - These demos and projects control the Robot directly from sensors connected directly to the Robot's control board.

Pose Control - These demos and projects allow you to create and playback a sequence of poses.

Serial Control - These demos and projects control the robot using a serial packet protocol.

Standalone - These demos and projects are deisgned to let your robot function without a computer or additional microcontroller.

Wireless Control - These demos and projects allow you to control the robot wirelessly - usually by replacing the Serial Connection with XBee modules.

Reference - These articles have technical details regarding the control and operation of the robot.

×

More info here

Arbotix Commander Assembly Guide

arbotixcommanderdone.jpg

Kit Parts List

1x b_400_400_16777215_00__images_assembly_arbotixcommander_arbotixcommander-bottomplate.jpg
Bottom Plastic Plate
1x b_400_400_16777215_00__images_assembly_arbotixcommander_arbotixcommander-topplate.jpg
Top Plastic Plate
1x b_400_400_16777215_00__images_assembly_arbotixcommander_arbotixcommander.jpg
Arbotix Commander Shield
1x b_400_400_16777215_00__images_assembly_parts_geekduino.jpg
Geekduino
2x b_400_400_16777215_00__images_assembly_parts_aa-batteryholder.jpg
AA Battery Holder

The following hardware is required to build the kit. You may have received extra parts with your kit.

18x bolt-m3-short.jpg
Hex Socket Head Bolt
M3 x 6
3x m3*10 ffstandoff
Hex Standoff F/F
M3 x 10
6x m3*30 ff stanoff
Hex Standoff F/F
M3 x 25
2x velcro-150-70.jpg
Velcro



Build Steps

Pre Step: Peel Your Plastic

Some of your plastic pieces will have paper masking on one or both sides. Peel the masking paper off before getting started.

There also may be some dust on your parts. This is from the laser cutting manufacturing process. It is harmless and can be cleaned up by wiping with a rag or being washed with water.


Step 1: Mount Standoffs to the Bottom Plate

9x bolt-m3-short.jpg
Hex Socket Head Bolt
M3 x 6
3x m3*10 ffstandoff
Hex Standoff F/F
M3 x 10
6x m3*30 ff stanoff
Hex Standoff F/F
M3 x 25

b_400_400_16777215_00__images_assembly_arbotixcommander_Img8769.jpg
Img8769.jpg
  • Mount standoffs to the Bottom Plate as shown using 3 x M3*10 Standoffs, 6 x M3*25 Standoffs, and 9 x M3*6 bolts.
  • Make sure you mount the standoffs with the shiny side facing up.

Step 2: Mount the Geekduino

3x bolt-m3-short.jpg
Hex Socket Head Bolt
M3 x 6

b_400_400_16777215_00__images_assembly_arbotixcommander_Img8771.jpg
Img8771.jpg Img8783.jpg
  • Mount the Geekduino using 3 x M3*6 bolts.
  • Make sure to set the Geekduino switches. The Reset switch needs to be on AUTO and the voltage switch needs to be on 3V3.

Step 3: Mount the Arbotix Commander Shield


b_400_400_16777215_00__images_assembly_arbotixcommander_Img8772.jpg
Img8772.jpg
  • Mount the Arbotix Commander Shield onto the Geekduino.

Step 4: Mount the Battery Holders

2x velcro-150-70.jpg
Velcro


b_400_400_16777215_00__images_assembly_arbotixcommander_Img8773.jpg
Img8773.jpg
  • Mount the Battery Holders as shown using the sticky backed velcro strips.
  • Plug the connectors into the Arbotix Commander.
  • NOTE: The +/- silkscreen on the left battery holder is incorrect. Plug the left battery pack into the commander normally (as indicated by the notch in the white JST connector.) The black wire will be toward the top of the commander (+ silkscreen) and the red wire will be towards the bottom (- silkscreen)
  • NOTE: Older versions of the Commander came with 2.5mm nuts & bolts to mount the battery packs. If you have one of the older models use these to mount your packs.

Step 5: Put in the Batteries


b_400_400_16777215_00__images_assembly_arbotixcommander_Img8775.jpg
Img8775.jpg
  • Put in the Batteries.
  • Check to make sure that the power is switched off so you don't leave your Commander on draining the batteries!

Step 6: Put on the top Plate

6x bolt-m3-short.jpg
Hex Socket Head Bolt
M3 x 6

b_400_400_16777215_00__images_assembly_arbotixcommander_Img8778.jpg
Img8778.jpg
  • Put on the Top Plate using 6 x M3*6 bolts.

Step 7: Mount the XBee


b_400_400_16777215_00__images_assembly_arbotixcommander_Img8781.jpg
Img8781.jpg
  • Mount the XBee into the XBee socket.