×

PC Control These demos and projects allow the robot to be controlled via a computer.

ArbotiX Commander Control - These demos and projects control the Robot using the ArbotiX Commander, the handheld Arduino based remote control.

Direct Control - These demos and projects control the Robot directly from sensors connected directly to the Robot's control board.

Pose Control - These demos and projects allow you to create and playback a sequence of poses.

Serial Control - These demos and projects control the robot using a serial packet protocol.

Standalone - These demos and projects are deisgned to let your robot function without a computer or additional microcontroller.

Wireless Control - These demos and projects allow you to control the robot wirelessly - usually by replacing the Serial Connection with XBee modules.

Reference - These articles have technical details regarding the control and operation of the robot.

×

More info here

WidowXL Robot Arm Getting Started Guide

This guide will help you get up and running with your WidowXL Robot Arm. By the end of this guide, you will have configured your robot electronics, assembled your robot and tested your robot. You will then be able to proceed to our demo code guides.

Setting Up Your ArbotiX & Arduino Software

ArbotiX Getting Started Guide

InterbotiX Kits are designed to work with the ArbotiX-M Robocontroller, an Arduino compatible microcontroller designed to work with DYNAMIXEL servos. This guide will show you how to setup and program the ArbotiX-M Robocontroller.

Setting Your DYNAMIXEL IDs

DYNAManager Software Guide

Every DYNAMIXEL servo comes set to a default ID of '1'. However, for your robot to work, you will need to set the servos to the correct ID numbers. This guide will help you use the DYNAmanager software and the ArbotiX-M robocontroller to set the IDs for each servo.

Each servo must be IDed one-at-a-time, so it is easiest to set the servo IDs before you assemble your robot. If you have multiple servos with the same ID connected to each other, you will not be able to ID the servos.

Servo ID Servo Model Horn and Idler configuration Servo Location
Servo ID #1: MX-28 Horn only Base
Servo ID #2: MX-106 Horn and Idler Shoulder
Servo ID #3: MX-106 Horn and Idler Elbow
Servo ID #4: MX-64 Horn and Idler Wrist Angle
Servo ID #5: AX-12 Horn only (preinstalled) Wrist Rotate
Servo ID #6: AX-12 Horn only (preinstalled) Gripper
servoIDlayout.jpg

Building Your Robot

Assembly Guide

This guide will show you how to build and wire your robot. This guide includes a list of parts that come with your kit and tips for building your robot.

Testing Your Robot

Build Check / Test Program

This guide will show you how to load a test program onto your robot as well as a video showing how your robot should move when the program is loaded. This test program and video will ensure that you have assembled your robot correctly.

Optional ArbotiX Commander / Wireless Setup

Configuring XBee modules
Setting up the ArbotiX Commander
WidowX Robot Arm / Arbotix Commander Demo Guide

If you have purchased the ArbotiX Commander and wish to control the arm via XBee modules, you will need to follow the instructions in the guides: Configuring XBee Modules and Setting up the ArbotiX Commander. Once you've completed setup for these devices, you can proceed to the WidowX Arm / Arbotix Commander Demo Guide

Optional Using LiPo Batteries

Working with LiPo Batteries

The WidowX Robot Arm can be powered from any 11-12v DC source. This includes batteries like Lithium Polymer (LiPo) batteries sold by Trossen Robotics. LiPo batteries need more care and attention than other rechargeable batteries. Please follow this guide to learn how to properly use, recharge and store your batteries.

Demo Code Guides

Demo Code

Now that you've finished setting up your robot, you can proceed to trying our demo code.

Projects

WidowX Robot Arm Projects

Once you have gotten comfortable with the demo code for your robot, check out some of the projects for your robot.