×

PC Control These demos and projects allow the robot to be controlled via a computer.

ArbotiX Commander Control - These demos and projects control the Robot using the ArbotiX Commander, the handheld Arduino based remote control.

Direct Control - These demos and projects control the Robot directly from sensors connected directly to the Robot's control board.

Pose Control - These demos and projects allow you to create and playback a sequence of poses.

Serial Control - These demos and projects control the robot using a serial packet protocol.

Standalone - These demos and projects are deisgned to let your robot function without a computer or additional microcontroller.

Wireless Control - These demos and projects allow you to control the robot wirelessly - usually by replacing the Serial Connection with XBee modules.

Reference - These articles have technical details regarding the control and operation of the robot.

×

More info here

WidowX Robot Turret Demos

  • Analog Joystick Control for the WidowX Robot Turret

    Description

    mt_ignore
    Standalone
    mt_ignore
    Direct Control

    The easiest way to control the Robot Turret is via the included joystick. This page will show you how to wire your joystick to your ArbotiX robocontroller and what code to load onto the ArbotiX Robocontroller.

    This code for this demo project will read the analog value from the joysticks, convert the raw value into a value ready for the DYNAMIXEL servos, and then write the positions to the servos. The code will also impose angle limits on the pan/tilt system and offer variable speed, adjustable by the user.

    The vertical joystick will control the tilt servo while the horizontal joystick will control the pan servo. These motions can be swapped in code, or by physically swapping out the 2 sensors. This code can work with a wide variety of joysticks. It can also work with other analog sensors, though some code modifications may be necessary depending on the desired behavior.

    Read More
  • Wireless Handheld Control for the WidowX Robot Turret

    Description

    mt_ignore
    Wireless
    mt_ignore
    Serial Control
    mt_ignore
    ArbotiX Commander Control

    The PhantomX RobotTurret can be controlled wirelessly via the ArbotiX Commander. In this demo, the ArbotiX Commander's joysticks will be mapped to the pan/tilt servos, and the pushbuttons will move the turret to pre-set positions.

    Users can modify the ArbotiX Robocontroller firmware in a variety of ways. The speed of the servos can be changed and the preset positions can be altered. Users can even trigger digital outputs (like relays) based on ArbotiX Commander input.

    Read More
  • DYNAPose - DYNAMIXEL/ArbotiX Pose Tool

    Description:

    mt_ignore
    Pose Playback
    mt_ignore
    PC Control

    All the InterbotiX robots turrets, arms, and crawlers use DYNAMIXEL servos. These servos all have positional feedback, allowing the ArbotiX-M Robocontroller to read the current position of each servo. This makes it possible to physically pose an InterbotiX robot, then capture the positions for each servo, allowing the user to save/capture the current pose. By capturing multiple poses, a user can create a sequence that can be repeated.

    This firmware does not use any Inverse Kinematic calculations to position the servos - it simply moves the servos to a pre-set position. Please see the 'Demo' section for your Robot for more information on code examples that us IK engines.

    Read More
  • Untethered Pose Playback with DYNAMIXEL/ArbotiX

    Description:

    mt_ignore
    Pose Playback
    mt_ignore
    PC Control
    (Setup Only)
    mt_ignore
    Standalone

    The ArbotiX-M Robocontroller can be used to easily 'play' a sequence of poses on DYNAMIXEL servos. These poses can run automatically, triggered by an outside input (like a pushbutton) or integrated into more advanced code.

    This tutorial can be used in conjunction with the DYNApose tutorial. The DYNApose tutorial will help you to capture a series of poses while this tutorial will help you integrate those poses into new code.

    This firmware does not use any Inverse Kinematic calculations to position the servos - it simply moves the servos to a pre-set position. Please see the 'Demo' section for your robot for more information on code examples that use IK engines.

    Read More
  • LIDAR Lite Mapping with DYNAMIXEL Servos

    This demo will show off the capabilities of the LIDAR Lite by rotating the LIDAR lite and using the data to create a visual map of the room. This demo will require Google Chrome to be installed on your computer.

    Read More